Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: LAUNCHXL-F28379D, MOTORWARE, BOOSTXL-3PHGANINV, C2000WARE-MOTORCONTROL-SDK
Tool/software:
We are designing a motor control system and have the following goals:
- PMSM or IPM motor
- FOC
- Normal operation and regen
- Speed or torque control
- Probably using quadrature sensor but we would like to evaluate sensorless
- Use MATLAB and Simulink for control system evaluation, simulation, tuning, and possibly code generation
- Maximum voltage <60 Vdc
- Maximum current 20-30 amps
- We have additional requirements but I cannot disclose them on a public forum
To start, MATLAB recommended the LAUNCHXL-F28379D and BOOSTXL-DRV8305. I'm not sure if these are the best options for our requirements. It's also unclear from the TI website which toolset is best: InstaSPIN-FOC, InstaSPIN-MOTION, MOTORWARE, MotorControl SDK, or something else.
- Is the C2000 series our best option?
- Do you recommend the LAUNCHXL-F28379D?
- Do you recommend the BOOSTXL-DRV8305? For initial development and evaluation, we could loosen our requirements.
- Should we consider the BOOSTXL-3PHGANINV or something else?
- Which development tools do you recommend?
Thanks,
Nat