Hello,
I have been evaluated F28335 eZdsp. I have problem about ADC.
I use external reference (JP1 is shorted, 2.048V) on ADCREFIN.
The conversion result is as follows.
Input Result
0.5V 0.50V
1.0V 0.95V
1.5V 1.40V
2.0V 1.88V
2.5V 2.33V
If the input is 2.5V, 2.47V is obtained approximately, I think.
If I have created a user board, I can get 2.47V?
I hope someone tell me your experience or information.
Best regards,
Nathan Morgan