This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: ADCIN14 and ADCIN15

Part Number: TMS320F28379D


Tool/software:

Hi,

I was exploring the possibility of using ADCIN14 and ADCIN15 for general purpose analog measurement. The reference manual mentions that these pins are connected to all ADC  (A, B, C and D). I was able to successfully test the feedback using the channel on multiple channels. What happens when the channels are called by channels with different configuration? ADCA is differential mode and ADC B is single-ended. I was able to read correct values based on the configuration of the ADCs - I had to use an SOC in each of the ADCs ( A and B) with the channel set to 14.  Is there any fundamental problem with using the ADCIN14 and ADCIN15 in this way, I was not able to find any documentation to suggest that it was a problem to use these as general purpose ADC inputs.? 

Thanks,

Aditya