This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to use TIDM-1000 "pfc3phvienna_F2837x" code on "TMDSCNCD28379D", I launch main.syscfg, all rectifier parameters such as inductance values, RC sense filter values, voltages etc. are defined, I can change them.
When I click "Device Vİew" I get "F28004x (Device) F28004x_100PZ (Part)" and I think that I should change it to "F28379D".
How can I change it and should I define PWM, ADC, GPIO pins according to "Table 2. Key Controller Peripherals Used for Control of Power Stage on Board" in "Design Guide: TIDM-1000 TIDUCJ0G–November 2016–Revised April 2020" ?
Regards,
Vedat
Hi Vedat,
in the properties section remove F28004x. This is causing the overwrite on sysconfig device name. This doesnt impact any of peripherals etc...
Best Regards,
Uttam