Part Number: TMS320F280025C
Tool/software:
Hello,
We are working on solar power pump design based on based on TMS320F280025C and universal motor control lab, we need help with one issue.
We are controlling the speed of the pump based on MPPT of solar panel and the pump is able to operate at optimal MPPT point, but when sudden load is applied the panel voltage is dropping quickly trigging under voltage protection.
We are able to detect the drop in panel voltage and trying to adjust the reference speed to match the available power but before the speed is reduced under voltage is condition is triggered.
Is there a way to quickly reduce the current drawn by motor to avoid folding of solar panel voltage or is it advisable to set current limit.