Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Tool/software:
Hi,
I'm using the CLA to read out two SPI encoders and so far that works fine. Not that I had to include some calibration routines, the code grew more and more and I'm now in the situation to use 4 RAM LS banks in total (3 for the program, 1 for the data), but this seems not to work out, I always get the following compiler error:
"program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. load placement with alignment/blocking fails for section "Cla1Prog" size 0x10dc page 0. Available memory ranges"
Now I don't understand the issue, since I could successfully merge RAMLS1 and RAMLS2 to a bigger bank, but it seems I cannot merge LS1-LS3 to a bank without this issue.
f28003x_flash_lib_is:
...
RAMLS012 : origin = 0x008000, length = 0x001800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLSnP : origin = 0x00A000, length = 0x002000
RAMGSnP : origin = 0x00C000, length = 0x001000
RAMGSC : origin = 0x00D000, length = 0x001000
RAMGSF : origin = 0x00E000, length = 0x001000
RAMGSD : origin = 0x00F000, length = 0x000FF8
...
// CLA Sections
#if defined(__TI_EABI__)
/* CLA specific sections */
Cla1Prog : LOAD = FLASHBANK1_CLA,
RUN = RAMLS012,
LOAD_START(Cla1ProgLoadStart),
RUN_START(Cla1ProgRunStart),
LOAD_SIZE(Cla1ProgLoadSize),
ALIGN(8)
.const_cla : LOAD = FLASHBANK1_CLA,
RUN = RAMLS3,
RUN_START(Cla1ConstRunStart),
LOAD_START(Cla1ConstLoadStart),
LOAD_SIZE(Cla1ConstLoadSize),
ALIGN(8)
#else
/* CLA specific sections */
Cla1Prog : LOAD = FLASHBANK1_CLA,
RUN = RAMLS012,
LOAD_START(_Cla1ProgLoadStart),
RUN_START(_Cla1ProgRunStart),
LOAD_SIZE(_Cla1ProgLoadSize),
ALIGN(8)
.const_cla : LOAD = FLASHBANK1_CLA,
RUN = RAMLS3,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
ALIGN(8)
#endif
.scratchpad : > RAMLS3
.bss_cla : > RAMLS3
Cla1DataRam : > RAMLS3 //RAMLS3
cla_shared : > RAMLS3
CLADataLS1 : > RAMLS3
Cla1ToCpuMsgRAM : > CLATOCPU_MSGRAM
CpuToCla1MsgRAM : > CPUTOCLA_MSGRAM
Init for the CLA:
void MEMCFG_init()
{
//
// Initialize RAMs
//
MemCfg_initSections(MEMCFG_SECT_MSGCPUTOCLA1);
MemCfg_initSections(MEMCFG_SECT_MSGCLA1TOCPU);
while(!MemCfg_getInitStatus(MEMCFG_SECT_MSGCPUTOCLA1));
while(!MemCfg_getInitStatus(MEMCFG_SECT_MSGCLA1TOCPU));
//
// Configure LSRAMs
//
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS0, MEMCFG_LSRAMCONTROLLER_CPU_CLA1); //LS0 - LS2 needs to be for CLA --> Change in flash.cmd file
MemCfg_setCLAMemType(MEMCFG_SECT_LS0, MEMCFG_CLA_MEM_PROGRAM);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS1, MEMCFG_LSRAMCONTROLLER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS1, MEMCFG_CLA_MEM_PROGRAM);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS2, MEMCFG_LSRAMCONTROLLER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS2, MEMCFG_CLA_MEM_PROGRAM);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS3, MEMCFG_LSRAMCONTROLLER_CPU_CLA1);
MemCfg_setCLAMemType(MEMCFG_SECT_LS3, MEMCFG_CLA_MEM_DATA);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS4, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS5, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS6, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
MemCfg_setLSRAMControllerSel(MEMCFG_SECT_LS7, MEMCFG_LSRAMCONTROLLER_CPU_ONLY);
// Lock/Commit Registers
//
//
// Enable Access Violation Interrupt
//
//
// Correctable error Interrupt
//
MemCfg_setCorrErrorThreshold(0);
MemCfg_disableCorrErrorInterrupt(MEMCFG_CERR_CPUREAD);
}
Any Idea why this does not work? I also activated the compiler option "--gen_func_subsections = on", but without success.
Edit: I found a work around, but I'm not sure what the tradeoff is. When I'm using the following it works:
Works out:
Cla1Prog : >> RAMLS012 .const_cla : > RAMLS3
Does not work:
// CLA specific sections
Cla1Prog : LOAD = FLASHBANK1_CLA,
RUN = RAMLS012,
LOAD_START(_Cla1ProgLoadStart),
RUN_START(_Cla1ProgRunStart),
LOAD_SIZE(_Cla1ProgLoadSize),
ALIGN(8)
.const_cla : LOAD = FLASHBANK1_CLA,
RUN = RAMLS3,
RUN_START(_Cla1ConstRunStart),
LOAD_START(_Cla1ConstLoadStart),
LOAD_SIZE(_Cla1ConstLoadSize),
ALIGN(8)
So, what is the trade off when not using the lfash bank loader? Will this lead to problems somehow?