This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280049C: Not able to update XDS110 board

Part Number: LAUNCHXL-F280049C

Tool/software:

Hi Team,

I am trying to debug board with example given in SDK but while trying to launch in debug+program mode through CCS(version12.8.0.00012), it gives error saying firmware need to update. When I click to update it gives error again saying "An attempt to connect to the XDS110 failed." with probable reasons given in image.

I tried to update firmware using XDSDFU also as per "XDS110SupportReadMe.pdf" but while running command "xdsdfu -f firmware_3.0.0.31.bin -r" it detaches from the driver.

Following is the directory of XDS110.

Can you help what could be the issue for not updating the firmware in XDS110 ?

Regards,

Bhavin P