Tool/software:
Hi TI expert,
My customer use different ADC channels to sample the same DC voltage. And find conversion result of F28377's ADCINA0 channel have lower value compared to other channels. All channels' external circuits are the same shown as below. When the external circuit is disconnected, we test the impedance between ADCINxx pins and GND. Find only ADCINA0 channel's impedance is 30Kohm, all others are about 60Kohm.

Could you please help explain the possible reason? And what we can do to correct ADCINA0 channel's sample result?
BR,
Fengyu