Hi,
I'm using F28035 GPIO22 (set as GPIO already) with a 10k pull-up resistor (to 3.3v).
When it executes "GpioDataRegs.GPASET.bit.GPIO22 = 1;" there is no problem, but when it goes to 'GpioDataRegs.GPACLEAR.bit.GPIO22 = 1;', I test the GPIO22 Pin, the 3.3v High-level do not go to Low-level, but stay at about 2.9v... and the program (code) stops at "ESTOP0"...
I test it only with the pull-up resistor, there is no other connections; anyone may help me?
Thanks!
Regards,
Felix