Part Number: TMS320F2800157
Tool/software:
Hello,
May I have question about F2800157 function safety?
Question1
I think F2800157 have compliant SIL2 and "systematic capability" SIL3.
https://www.ti.com/lit/fs/sffs748/sffs748.pdf
Is this mean F280015x compliant SIL2 in only this chip, but SIL3 need external fail detection logic?
Or SIL3 certification require including software?
Question2
Is this certification including software? or only MCU hardware?
Question3
Do you have any application-note, guide, or manual for achieve the SIL3?
And It would be great if there is a manual on diagnostic methods.
Question4
I believe MTBF can see from TI HP.
However my customer require RAM, CPU, flash, permanent failure rate and temporary failure rate data for each peripheral.
May I get this data?
Thanks,
GR