This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: adc reference configuration

Part Number: TMS320F2800137

Tool/software:

Hi expert,

1. What is the routine software configuration of the internal reference 1p65 is 1.65V and the configuration of 3.3?

2. The example is configured so that the chip vrefH is not connected to 3.3v, the chip sampling is abnormal, and the sampling value is calculated according to the benchmark 1.65 according to the appeal configuration? Why do you need to connect this VREFH to 3.3 when configuring the internal reference?

Best Regards

Anka Zhang