This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28P650DK: About BiSS-C encoder and EnDat encoder support.

Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hi sir

I have a question about the encoder,

1) For the following paths in C2000Ware_MotorControl_SDK_5_02_00_00, confirm that only the tformat encoder is released and other encoder types are not released.

>> C:\ti\c2000\C2000Ware_MotorControl_SDK_5_02_00_00\solutions\boostxl_posmgr\f28p65x

2) Support for BiSS-C encoder and EnDat encoder is as follows:

Sample code is provided for the f2837xd BiSS-C encoder and nDat encoder.

f28p65x BiSS-C encoder boostxl_posmgr\f28p65x BiSS-C encoder support

But the f28p65x EnDat encoder and the f2838x BiSS-C/EnDat encoder are not provided. Can you provide sample code?

Thanks.