This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280025C: Replace the Arduino with the LAUNCHXL-F280025C

Part Number: LAUNCHXL-F280025C
Other Parts Discussed in Thread: BQ76952, , C2000WARE

Tool/software:

Hi Experts,

I use the bq76952 to monitor battery voltage, current, and temperature. Previously, I used an Arduino board to read data from the bq76952 via I2C and communicate with my PC through the CAN bus.

Now, I want to replace the Arduino with the LAUNCHXL-F280025C. Specifically, I would like to use this board to read data from the bq76952 via I2C and transmit the data to the PC through the CAN bus. Are there any software examples for the LAUNCHXL-F280025C that can accomplish these two tasks: 1. Configuring the bq76952 via I2C and continuously reading data from it? 2. Continuously sending the read data via the CAN bus.

Regards,

Josel