Tool/software:
Hi experts,
a customer is having an question of using SPI on the CLA, but let me forward the question:
Just wanted to ask you guys if it’s entirely possible to run SPI on CLA? I have come across a few posts on the TI forum about the CLA having access to SPI peripheral registers. In these scenarios SPI transactions were initiated by the CPU. So I’m not sure if it is really possible to offload the SPI on CLA.
Just to give you a background on our application. Basically we will be running two control loops on the CLA and since the built-in ADC doesn’t meet our requirements we will be using external ADCs. Basically we wanted to check with you if it is possible to have the CLA initiate SPI transactions with the external ADC. This way the readback is readily available for the control loops to use. Then we will just use either the CLA Data Memory or the CLA Message RAMs to transfer the ADC readbacks to the MCU for housekeeping tasks.
Kind regards,
Marinus