Part Number: TMS320F280037C
Tool/software:
We are currently experiencing unexpected resets with our F280037C microcontroller while operating around 80°C ambient temperature environment. We noticed that there was a loss of CAN communication for a period, which subsequently reestablished.
To diagnose the reset cause, we have gone through the RESC status register documentation and SysCtl_getResetCause(void) but are unsure how to read this information using CCS code or directly from memory. Any guidance on this would be greatly appreciated.
Additionally, we would like to understand the potential effects of high ambient temperatures on the reset behavior of the microcontroller.
For reference, we are using the following ICs to power the microcontroller:
- INN3166C-H101-TL
- TPS560430XDBVR
Any guidance on this would be greatly appreciated.