This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28P55X: CCS Project for Sensor-less FOC

Part Number: LAUNCHXL-F28P55X
Other Parts Discussed in Thread: BOOSTXL-3PHGANINV, LVSERVOMTR, C2000WARE, C2000WARE-MOTORCONTROL-SDK

Tool/software:

Hi,

I possess the following items:
1. Controller Board: [LAUNCHXL-F28P55X (TMS320F28P55x LaunchPad developm.)]
2. Inverter Board: [BOOSTXL-3PHGANINV (48-V/10-A three-phase GaN inverter)].
3. Supported Motor: Low Voltage Servo Motor - Low voltage servo (encoder) motor and wiring harness [LVSERVOMTR, P/N: M-2310P-LN-04K, Teknic M-2310P-LN-04K]

Also, I have installed Code Composer Studio (CCS Version: 12.8.0.00012) IDE for development and C2000Ware Software Development Kit (SDK Version: C2000Ware Motor Control SDK_5_02_00_00).

I was able to find only one example for the board f28p55x at the location given below which is for sensored foc:

C:\ti\c2000\C2000Ware_MotorControl_SDK_5_02_00_00\solutions\boostxl_3phganinv\f28p55x\cc 

             

I'm considering implementing sensor less FOC to control the motor. Can you assist me by supplying the necessary information and tools for this as listed below:

1) Configuration: Pin configuration.

2) Project Generation: Can you suggest a tool for creating code for sensor less field-oriented control, considering that the example is for a sensored system?

3) Debug Tool: Is there a tool available for adjusting motor speed, altering parameters, and real-time monitoring? If not, does this tool have support for modifying parameters through any configuration file?

Thanks, and regards,

Prasanth