Other Parts Discussed in Thread: TIDM-HV-1PH-DCAC, C2000WARE, PMP23069, PMP23338
Tool/software:
Dear Sir,
I'm working with the TIDM-HV-1PH-DCAC reference design using the C2000Ware Digital Power SDK 5.01.00.00 (I'm running the gridConnectedInverterCLFltr_F2837x solution).
I have couple of questions:
1. It seems I have an over c1urrent problem as I found that EPwm1Regs.TZFLG.DCAEVT1 is high and then happens two things: 1. the software logical sate changes to OFF 2. the TripZone hardware set the output line to low.
if I try to restart the run session the over current problem remains with the above symptoms. If I try to reset the EPwm1Regs.TZFLG.DCAEVT1 to low it doesn't change the situation.
can you suggest a reasonable logic to overcome this situation?
How can I change the threshold limit to allow higher current at the output?
2. I'd like to increase the frequency of the inverterISR to 100Khz (including the PWM rate). what are the changes (software/hardware) needed to be taken to establish this working condition? can you write the explicit changes which are required
Best Regards,
Tomer