Part Number: TMS320F2800157
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Is there MPOST support on this device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F2800157
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Is there MPOST support on this device?
This device does support MPOST, however, there is a bug in some production material that results in MPOST not running at boot, even if the proper OTP locations are written to enable it. Here is some additional information:
The OTP revision information is located at address 0x711DE. If you see a value >1 in lower 8-bits of this address then MPOST will work as documented. If you see 0 or 1 then above bug exists.
In this case we can give an alternate method of checking the goodness of the SRAM on the device, and that is to use the STA_MARCH test that is part of the F280015x SDL located in C2000Ware here: C:/ti/c2000/C2000Ware_5_02_00_00/libraries/diagnostic/f280015x/
This can be called as part of you main application, and will give equivalent coverage to the MPOST test.
Best,
Matthew