Part Number: TMS320F28P650DK
Tool/software:
Hi experts,
My customer is using F28P65 to develop EtherCAT project.
They are developing FOE function. So they need to use CCS to export the bin file. The features of bin file are as follows:
1. Size of bin file is the same with FLASH of F28P65. (Unused FLASH space is filled with F in the bin file)
2. Add the CRC check code at the end of the bin file.
Any suggestions for this issue?
Thanks,
Leo