Part Number: TMS320F28034
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi experts:
My customer need to use uniflash to connect with F28034 and they meet the issue as follows:
If he use "Create the session From existing Target configuration file"
he will meet:

if he use "Detected devices" or "New configuration"
he will meet:


However, My customer can use this ccxml file to connect to the F28034 by using CCS.
And we check the connection in CCS. The JTAG connection is OK.
On my side, I test the ccxml file, and I can connect to the device by using uniflash.
Any suggestions for this issue?
Details for my customer's PC and software
PC: windows 11 home 23H2
OS version: 22631.4317
Uniflash: 8.5.0 and 8.8.0 (Both of them meet the issue before)