Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi , I struggled the debug the program.
I imported the "can_ex3_external_transmit" project from "Resource Explorer".
When i launch the debug (from RAM or FLash) ,sometimes the breakpoint points the different places than i expected.
For example when i try to step into the CAN_sendMessage(), it jumps the somewhere in the CAN_setupMessageObject() function.
Board : TMS320F28388D controlCARD
CCS Version : 12.8.1.00005
Compiler Version : TI v22.6.1.LTS
Linker command file : 2838x_RAM_lnk_cpu1.cmd
Debugging Model : Full symbolic debug
Specify DWARF version : 4
Runtime Environment -> Initialization model : Link using autoinitializing model