This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Noah,
I still haven't seen the release of lwIP with the Concerto. Will it be out soon?
What is the closest Stellaris mircro to the Concerto ARM (like the 28335 for DSP)?
Thanks,
Tim
Tim,
I'm attaching a ported version of lwip. It's not on controlSUITE yet, but I hope it will help.
You will need to replace the MWare\third_party\lwip-1.3.2 directory with the included one. Make sure the enet_lwip project is placed in the appropriate directory (F28M35x_examples_Master).
5327.lwip.zip EDIT: Outdated File, see later post for updated version.
Let me know if you have any problems.
Alvaro
Tim,
Version 4.9.1 should be available if you check for updates on CCS.
You can also downgrade the codegen tool version by right clicking on the project->source->upgrade code generation tools version and set it to 4.6.6.
Let me know if that doesn't work.
Alvaro
Hi Alvaro,
My CCS auto update is not working, but I figured out how to do a manual update by manually pointing to the update web address, and was able to upgrade to Code Gen v4.9.1. I'm about to try the project you sent.
Thanks again.
Tim
Hi Alvaro,
I have built and ran the executable, and have not been able to get it to work, so I'm looking for more help.
Right now I'm testing using the Ping command from a laptop, and would like to see an echo response from the Concerto. I have made a few modifications to facilitate this.
In main( ), I added and changed:
IP4_ADDR(&ipaddr, 192,168,1,10);
IP4_ADDR(&netmask, 255, 255, 255, 0);
lwIPInit(pucMACArray, ipaddr.addr, netmask.addr, 0, IPADDR_USE_STATIC);
And in lwipopts.h, I uncommented:
Tim,
By default, the program attempts to acquire an IP address through DHCP. If it is unable, it selects a default one. If you're connecting it to a router, it should come work out of the box. If you're using a direct ethernet connection to your laptop, it's slightly different. Which are you using?
Also, a very helpful feature is the serial terminal. If you open up the virtual COM port that comes up when connecting via the USB cable to the controlCARD, some debug messages are printed. In the default caese, it will print out the DHCP acquired IP address, or the default one, if it comes to that.
Try running it as it was and see if it gets an IP. Once you have that, you can both ping it or access the sample web server with any browser.
Alvaro
I'm glad you got it working!
I found several bugs in the previous code. Here's the most up-to-date version. I forgot to initialize and load the code from flash, so the previous version won't work without the debugger.
Changed files are: setup_ccs.c, lwip.cmd, and enet_lwip.c
Alvaro
Hi.
I try to debug this lwip example with ccs 4.2.4.00033 (eval. 30-day license) and Sauris IsoPlus SAU510 JTAG emulator with latest drivers. The time passed from clicking "Debug Active Project" till "Run" button became available is over 10 minutes. Is it normally? I have to debug the project where lwip is just a part. This project was previously developed for Stellaris MCU under Keil software, but there are no Keil software for Concerto MCU. How to decrease the uploading and debugger starting time?