Part Number: TMS320F280049C
Other Parts Discussed in Thread: TMS320LF2406A
Tool/software:
Hi TI expert,
My customer use TMS320LF2406 and F280049 to communicate with the same CAN node. The node is special because its communicate rate is not stable, about 122kbps~128kbps.
F2406 and F280049's configuration are shown as below. Communication rate are 125kbps. Under this condition, they find F280049 will receive more error frame. We use calculation formula in F280049 TRM to calculate Oscillator Tolerance Range and F28004x has higher Oscillator Tolerance Range than F2406. So we can't understand why F280049 has more error frame.
Could you please help explain why F2406 receive little error fame? And what I we do to decrease the number of F280049's error frame? Thanks
|
PN |
CPU frequency |
SJW |
TSEG1 |
TSEG2 |
BRP |
Tq |
Bit-Time |
Oscillator Tolerance Range |
|
|
1 |
TMS320LF2406A |
40 |
3 |
11 |
4 |
20 |
500ns |
16 |
0.9375% |
|
3 |
TMS320F28004x |
100 |
4 |
9 |
6 |
50 |
500ns |
16 |
1.25% |
BR,
Fengyu