Part Number: TMDSCNCD28388D
Other Parts Discussed in Thread: C2000WARE, TMDSHSECDOCK,
Tool/software:
Hi,
We are currently running the CAN example for the CM from the template located at:
C:\ti\c2000\C2000Ware_5_03_00_00\driverlib\f2838x\examples\cm\can.
We didn't change anything, and the CAN bus bit rate was set to 500kHz (as default). However, it didn't communicate with the PeakCAN monitor. We then used an oscilloscope to monitor the CAN TX pin and found that the actual bitrate was 520kHz.
When we changed the bit rate as shown below, the PeakCAN started communicating, but the oscilloscope showed the actual bitrate to be 488kHz:
“CAN_setBitRate(CANA_BASE, CM_CLK_FREQ, 485000, 16);”Could you please help us resolve this issue?
Thanks a lot,
Rick