This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28054F: Application issues.

Expert 2340 points

Part Number: TMS320F28054F
Other Parts Discussed in Thread: MOTORWARE

Tool/software:

Hi Team,

Using TMS320F28054F, the software is ver1.01.00.18, and the lab02a of drv8312kit_devD in motorware
1. What is the reason for inputting 60V and then performing parameter recognition again after the parameter recognition is completed?
What is the usual recognition error?
2. Does parameter recognition support 400V? Parameters need to be identified for each component at a current of 100A.