Part Number: TMS320F28375D
Tool/software:
Hi experts,
My customer is trying to create a PFC power supply using the TMS320F2837xD, but is having issues with power consumption.
Q1: Are there any other ways to reduce power consumption besides the following?
・Change internal 1.2V generation from LDO to DCDC
・Set unused GPIO pins to output, disable internal pull-up, and disconnect external resistors
・Stop unused peripheral clocks
The measured microcontroller power consumption after these measures is about 0.45W.
The use of Low-Power Modes is not possible because they are considering reducing power consumption while the CPU is running.
They plan to consider "Flash is powered down" in the future.
When they ran a board similar to the PFC implemented in C2000 using the STM32G474QET6, the power consumption on the datasheet was about 0.1W, and the actual microcontroller temperature rise was lower than that of the C2000.
They would like to be able to reduce power to this level even with the C2000.
Best regards,
O.H