Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi TMS320F28P650DK6 champ !
A customer is currently developing a board using the C2000 TMS320F28P650DK6 device.
While downloading the firmware via UNIFLASH, they encountered 2-3 errors while erasing the flash.
After that, when they tried to download the firmware again via UNIFLAHS, it would get an FMSTAT error and it would not download.
The firmware is currently being used as a flash boot, and the code is starting at FLASHBANK0 (0x080000),
When downloading via UNIFLASH, it is clearing all flash areas (FLASHBANK0~4) and downloading.
However, when they clear the remaining areas except FLASHBANK0, the flash areas are being cleared normally as before.
I would like to know if there is any solution or something I need to check for the above situation.
Thanks.
Best Regards,
Jack