Part Number: TMS320F28384S
Tool/software:
Hi Team,
we have recently procured 28384s ICs to replace with 28377s ICs with same hardware (Only change is 56 Ohm resistor placed between VDD and VSS in place of the decoupling capacitor). I have gone through migration guide and made the project for 28384s. Even with any of the example projects run with flash or RAM linker files also same issue.
I am able to flash the code and connect the emulator but application code is not running. I am thing its stuck in boot mode itself. GPIO72 & GPIO84 connected 3.3V through 4.7k pullups so both are always high so flash boot mode will be selected as it is already programmed once.
When I checked XRSn pin its getting low every 14.44ms once with 52us low.
Kindly check the screenshots attached for the reference