Part Number: TMS320F28P550SJ
Other Parts Discussed in Thread: TIDM-02011
Tool/software:
Hi Champ,
I am asking for my customer.
For live update feature, the bank0 and bank1 use different flash address offset. While this is not convenience for user because they need to prepare two special hex special for bank0 & bank1. In production field, user can not decide which bank the product is using because different version product have different bank usage condition.
(1). As spruiu8a shown, F28P55X uses the same logic, correct ?
(2). If user wants to use one image fit to two banks, do we have any solution to ease the implementation in production field ?
(3). TI compiler can help to decide which variable is preserved. Is there a piece of demo source code & detailed doc. could provide to customer for evaluation ?
Thanks and regards,
Johnny