Part Number: TMS320F28P650DH
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi Champs,
Now customer test C:\ti\c2000\C2000Ware_5_04_00_00\libraries\communications\Ethercat\f28p65x\examples\f28p65x_cpu1_echoback_solution. And use F28P65 LaunchPad. Boot mode is flash boot.
And have below questions:
1. When set configuration to "LAUNCHXL_FLASH", debug will have error.


2. When set configuration to "FLASH"

If the disable optimization level, the communication is correct. If the optimization level is enabled, when debugging online with CCS, everything works fine. But after the board is powered off and re-power on, the master station cannot scan the slave node.

After testing, customer suspected that the following two sentences were not working correctly.

Could you please help to check this? Thanks!
Julia