This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28P65X: Programming Error Message

Part Number: TMDSCNCD28P65X
Other Parts Discussed in Thread: C2000WARE

Tool/software:

Hi Team,

A customer is trying to program the TMDSCNCD28P65X, and has imported the example from C2000Ware_5_02_00_00\driverlib\f28p65x\examples\c28x_dual\led but when they try to program the console it throws the following message:

IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 12.7.0.00105)

They also ran a test connection using the test connection features on CCS and the result was as follows: SC_ERR_XDS110_OPEN (The full log is attached to this email).

Can you please suggest some fixes to this issue?