This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Problem During The Debug The BootROM

Part Number: TMS320F28388D

Tool/software:

Hi folks,

After i connected the board over debug interface, i load the Run -> Load -> Load Symbols -> F2838x_CPU1_ROM_Aug_16_2019.out
and then Run -> Reset -> CPU Reset.

When the program reaches the "LCR CPU1BROM_startSystemBoot"(cpu1brom_init_boot.asm) problem was begin,
If i click "Assembly Step Over" the CCS stucked , didn't respond anything.
If i click "Assembly Stemp Into", the program reaches "SB $C$L75, UNC", it didn't continue and core registers didn't change also.

What i need to do properly for debug the BootROM?

Best regards.