Part Number: TMS320F28027F-Q1
Other Parts Discussed in Thread: TMS320F28027F, C2000WARE
Tool/software:
Hello,
I am using the TMS320F28027F, and I would now like to download software via the UART interface from a running application. Normally, you would use the external pins to set the boot mode (here UART) and execute a reset so that the CPU goes into boot mode. Can I initiate a bootload from the serial interface from a running application (is it even possible without setting an external boot vector)?
best regards
Thomas