Tool/software:
Hi team:
We need to implement Flash ECC self-test, and also use hook function to implement MPU. Here is the configuration of the hook function in properties.

We clear uncorrectable error status(MemCfg_clearUncorrErrorStatus(MEMCFG_UCERR_CPUREAD)) in nmiISR. We put nmiISR interrupt function in RAM. The code runs out of control when executing EALLOW in MemCfg_clearUncorrErrorStatus function. Here is the position where code runs out of control in debug mode. But it executes normally without hook function. Why?


BR
Samuel