This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: Adding files in CCS project

Part Number: TMS320F280049

Tool/software:

Hi Team,

I have a CCS project and I manually add a file to the project. When I update the project through command line, the added file is not accessible.

When adding the file if I had linked the file, then on project update the linked file does not show up and I have to manually add again.

When adding the file if I had copied the file, then the file is present but on accessing the file it throws error saying file does not exist.

Kindly let me know if there is a way I can add the file to a project and it will remain in the project even when I update the project through command line.

Kind regards,

Irene

  • Hi Irene,

    Can you share the exact steps you follow to update the project through the command line? Something that is replicable would help debug this further. Do you see the new file within the project's directory?

    Best,

    Ryan Ma