Part Number: TMS320F28379D
Tool/software:
I am attaching photo of First control card showing its setup of A:SW1 and SW1, and I am connecting to it using using XDS100v2 onboard emulator.
I don't see any PWM outputs and the program is running from Flash. Surely, I have tried restarting the control card. The control card outputs PWM when I run the program from RAM instead of downloading it to FLASH. I have also removed R83 but no luck for getting the PWM to output that is measured using oscilloscope. The second control card has the same issue.
There is a third control card with setup, A:SW1 is set as 1 ON (up) and 2 OFF (down) and SW1 : 1 UP AND 2 UP. This control card works fine and outputs PWM. R83 is not removed from this control card. I have tried this configuration on the other control cards too.
Could you please help in fixing the issue?