This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F2800137: Trying run a gpio toggle example and debug unable to do.

Part Number: LAUNCHXL-F2800137


Tool/software:

Hi, 
I am new to TI products. I have a LAUNCHXL-F2800137 board with me. 
I downloaded CCS Theia 1.5.1. and connected the board via USB to Type-C cable.
The issues I am getting are below.

1. When I powered the board the CCS theia did't detect the board.
2. I manually selected the board and example and tried to run it says the following error


Texas Instruments XDS100v2 USB Debug Probe/IcePick_C_0 Error connecting to the target: (Error -716 @ 0x0) Required dynamic library jscserdes could not be located. The library isn't on the search path. (Emulation package 20.0.0.3178)


Also in device manager on ports the XDS110 usb probe is not showing.
 

Thought the driver would have downloaded along with the software or when I give debug first time it would have download but not I thjink so.

Kindly let me know how to overcome this issue also provide link or file for xds110 driver

Thanks in advance

Sai