I am trying to embed the TMS320F28335 control card in a power converter, and use the SCI communication interface. Upon examining the control card schematic, an onboard RS-232 chip connects the transmit and receive signals. I need to use RS-485 for my application. Do I need to use an RS-232 to 485 converter or can I directly connect the Tx and Rx signals to the RS-485 IC?
Thanks!
-Adithya