Other Parts Discussed in Thread: TMS320F28335
Hi all, I am facing some problems when I try to change the XCLKOUT of TMS320F28335. Acctually I just get an XCLKOUT of 75MHz no matter the settings I put on the XTIMCLK and CLKMODE bits of the XINTCNF2 register. I tried using the XCLKOUTDIV bit of the XCLK register but it seems that this register does not exit anymore in TMS320x2833x. I'm using the SYSCLKOUT of 150Mhz so normally this should work properly but it seems that I'm missing something. Thanks