Part Number: LAUNCHXL-F28P65X
Other Parts Discussed in Thread: SFRA, C2000WARE
Tool/software:
Howdy, I am currently getting the warnings of (#10247-D creating output section "MSGRAM_CPU1_TO_CPU2" without a SECTIONS specification) & (#10247-D creating output section "MSGRAM_CPU2_TO_CPU1" without a SECTIONS specification) after porting the Universal Motor Control Lab.
Here is my flask_lnk file
MEMORY
{
BEGIN : origin = 0x080000, length = 0x000002 // Update the codestart location as needed
RAMM0S : origin = 0x000128, length = 0x000158
RAMM1D : origin = 0x000280, length = 0x000578
RAMLS4 : origin = 0x00A000, length = 0x000800
RAMLS567 : origin = 0x00A800, length = 0x001800
RAMGS0 : origin = 0x010000, length = 0x002000
FLASHBANK0_BOOT : origin = 0x080002, length = 0x00800
FLASHBANK0_CODE : origin = 0x081000, length = 0x00D000
FLASHBANK0_DATA : origin = 0x08E000, length = 0x001000
FLASHBANK0_PRMS : origin = 0x08F000, length = 0x000FF0
RESET : origin = 0x3FFFC0, length = 0x000002
}
SECTIONS
{
.reset : > RESET, TYPE = DSECT /* not used, */
codestart : > BEGIN
.text : > FLASHBANK0_CODE,
ALIGN(8)
GROUP
{
.TI.ramfunc
ramfuncs
dclfuncs
dcl32funcs
}
LOAD > FLASHBANK0_CODE,
RUN > RAMLS567,
LOAD_START(RamfuncsLoadStart),
LOAD_END(RamfuncsLoadEnd),
LOAD_SIZE(RamfuncsLoadSize),
RUN_START(RamfuncsRunStart),
RUN_END(RamfuncsRunEnd),
RUN_SIZE(RamfuncsRunSize),
ALIGN(8)
ctrlfuncs : LOAD > FLASHBANK0_CODE,
RUN > RAMLS567,
LOAD_START(loadStart_ctrlfuncs),
LOAD_END(loadEnd_ctrlfuncs),
LOAD_SIZE(loadSize_ctrlfuncs),
RUN_START(runStart_ctrlfuncs),
RUN_END(runEnd_ctrlfuncs),
RUN_SIZE(runSize_ctrlfuncs),
ALIGN(8)
.binit : > FLASHBANK0_DATA,
ALIGN(8)
.cinit : > FLASHBANK0_DATA,
ALIGN(8)
.stack : > RAMM0S
.init_array : > FLASHBANK0_CODE,
ALIGN(8)
.bss : > RAMM1D
.const : > FLASHBANK0_CODE,
ALIGN(8)
.data : > RAMM1D
.switch : > FLASHBANK0_CODE,
ALIGN(8)
.sysmem : > RAMM1D
est_data : > RAMLS4,
LOAD_START(loadStart_est_data),
LOAD_END(loadEnd_est_data),
LOAD_SIZE(loadSize_est_data)
hal_data : > RAMM1D,
LOAD_START(loadStart_hal_data),
LOAD_END(loadEnd_hal_data),
LOAD_SIZE(loadSize_hal_data)
user_data : > RAMM1D,
LOAD_START(loadStart_user_data),
LOAD_END(loadEnd_user_data),
LOAD_SIZE(loadSize_user_data)
foc_data : > RAMM1D,
LOAD_START(loadStart_foc_data),
LOAD_END(loadEnd_foc_data),
LOAD_SIZE(loadSize_foc_data)
sys_data : > RAMM1D,
LOAD_START(loadStart_sys_data),
LOAD_END(loadEnd_sys_data),
LOAD_SIZE(loadSize_sys_data)
vibc_data : > RAMGS0,
LOAD_START(loadStart_vibc_data),
LOAD_END(loadEnd_vibc_data),
LOAD_SIZE(loadSize_vibc_data)
dmaBuf_data : > RAMGS0,
LOAD_START(loadStart_dmaBuf_data),
LOAD_END(loadEnd_dmaBuf_data),
LOAD_SIZE(loadSize_dmaBuf_data)
datalog_data : > RAMGS0,
LOAD_START(loadStart_datalog_data),
LOAD_END(loadEnd_datalog_data),
LOAD_SIZE(loadSize_datalog_data)
SFRA_F32_Data : > RAMGS0,
LOAD_START(loadStart_SFRA_F32_Data),
LOAD_END(loadEnd_SFRA_F32_Data),
LOAD_SIZE(loadSize_SFRA_F32_Data)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
This project only uses cpu1 and I am unsure how to resolve these warnings.
Please let me know if any additional information is needed.
-Thanks