Part Number: TMS320F280025C
Other Parts Discussed in Thread: DRV8316
Tool/software:
Hii everyone
i'm running bldc motor using TMS320F280025C + DRV8316 EVM refering " Motor Control SDK Universal Project and Lab doc". www.ti.com/.../spruj26a.pdf and i"m at step 3 on 3.5.1.3 where it says "In the Expressions window, set the variables motorVars_M1.flagEnableRunAndIdentify to 1 after systemVars. flagEnableSystem was automatically set to 1 in the watch window." but im not able to put value in expression window default the value is 0'/x00' if i press 1 and than hit the enter key ,value remains the same is that anything im missing.