Tool/software:
Sirs ... our engineering group independently have the same problem in THEIA 1.5.1 latest with missing INCLUDE file group when performing the following actions.
File>Project IMPORT>Open 'Resource Explorer'>Select LaunchXL F280039C>select 'epwm_ex9_dma' >CREATE>expand project &=no INCLUDE files.
Then looking at the workspace directory ...even the basic one "Workspace_CCSTHEIA" I cannot see any filenames related to an INCLUDE function.
I have a number of people waiting to employ Theia which so far has functioned really well ... we have unuinstalled and download the zip and re-installed twice on TWO MSoft10/11 PC's.
The .log file showing what appear to be "segment" errors at TI server is on my last post with Susmitha ...
Resolution of this issue would really be welcome - I was sure I had doe something silly ... but it really looks like a THEIA IDE issue ???