This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28027F: Why does my motor not work using lab11?

Part Number: LAUNCHXL-F28027F

Tool/software:

I am working on a project where I am using my own hardware circuit to drive a motor.

When using the instaspin_labs routine, the motor worked fine using lab1-lab11,

but starting from lab11, the motor stopped turning properly. The motor vibrates back and forth, and the current becomes very large.

The 6 mosfets also become very hot. I tried changing several parameters, but none of them solved the problem.

What should I do?

Attached is my user.h file

5758.user.h