Part Number: TMS320F280034
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Tool/software:
Hi,
Working on our next servo drive based on TI microcontroller (started a long time ago with F241, latest was F28069).
Using CCS 12.8.1.00005, XDS100v3 probe.
Imported "led_ex1_blinky" sample project and only changed the target configuration, linker files are not modified.
The RAM configuration loads and runs/debugs without any issues.
The FLASH configuration displays the following at loading:
C28xx_CPU1: GEL Output:
RAM initialization done
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
C28xx_CPU1: File Loader: Verification failed: Values at address 0x080000@Program do not match Please verify target memory and memory map.
C28xx_CPU1: GEL: File: E:\4Work\Software\NewDSP_CCS12.8\0test1\led_ex1_blinky\CPU1_FLASH\led_ex1_blinky.out: a data verification error occurred, file load failed.
The same happens with all other sample projects I tested.
When running the RAM configuration, the memory browser displays all FFFFs starting at address 0x080000.
Can you please help!
Regards,
Vesko Vitchev