This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Serial Flash Programmer Through SCI and OTP

Part Number: TMS320F28379D

Tool/software:

Hello There,

I am currently working on serial flash programming with TMS320F28379D. I've looked at this document and configured GPIO72 -> 0 and GPIO84 -> 1 . I configured SCI boot mode with this configuration. At default, SCIA uses GPIO84 and GPIO85. I have a question about this topic.

  1. If I configured GPIO28 and GPIO29 at OTP BMODE bitfield, I will not be able to reprogram again the MCU. So, If I just use default configuration which is GPIO84 and GPIO85 for SCI and program the MCU,  am i going to be able to reprogram the MCU?

Yasin