This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Trigger CLB from FSI RX when receiving a frame

Part Number: TMS320F280049C

Tool/software:

Hi Support Team,

in "Figure 28-2. FSI Receiver (FSIRX) CPU Interface with CLB" in the FSI chapter of the F280049C spec (SPRUI33H), there is a connection from the FSI RX module to the CLB. Four types are specified: FSIRXyDF,  FSIRXyEF, FSIRXyPF and FSIRXyTAG. We are especially interested in FSIRXyPF to trigger the CLB when a FSI Ping Frame is received.

Sadly later in the chapter "28.3.3 FSI Receiver Module" there is no hint of this feature. The connection from FSI RX to CLB is missing completely in "Figure 28-5. FSI Receiver Block Diagram" and also in the description. Also I wasn't able to find any more information in the CLB or the SCI chapters.

Is it possible to trigger the CLB directly when receiving certain FSI Frame Types?

Thanks a lot and best regards,
Oliver