Part Number: TMS320F28335
Tool/software:
Hi,
I am working on TMS320F28335, having configuration file and out file to load the program using C2000 Series XDS510LC JTAG Emulator. I have below problems, any help will be apricated as I got stuck and production got hampered.
1. TMS320F28335 is not programmed as I have used many times but now target not connected and Device is locked like prompts are coming in different PCs and Laptop.
--> I have checked all the signals of JTAG and RESET and all power supplies they are OK now JTAG is not connected with emulator.
--> Should I have used different programmer and CCS version as current version is 5.5.
--> Also I have tried with new mounted chip but results are same. so I have doubt on c2000 emulator but still I have same result with other one also.
Please suggest if any one have any idea upon that also any other programmer which can be used to program it.
Regards
Gaurav