This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: Question

Part Number: TMS320F28069M

Tool/software:

I tried deploying my Simulink model to a TI F28069 hardware board, but I received an error saying, 'Error occurred during deployment to the hardware board. Check the "Download Executable to Hardware" stage above for more details.'

After checking the hardware setup, I noticed that the hardware board is not recognized in the Device Manager, meaning the port connection seems to be missing or incorrect. This might indicate an issue with the USB driver or the connection itself.

I have already tried verifying the hardware configuration in Simulink, checking the USB cable, and ensuring the required support packages are installed in MATLAB. However, the problem persists.

Could you suggest how I can resolve the issue with the Device Manager not detecting the hardware? For example, do I need to install a specific driver for the board, or is there a setting I should adjust in Windows or Simulink? Your guidance would be greatly appreciated."