Part Number: TMS320F28035
Tool/software:
If I have more than 3 interrupt external signals that are connected to GPIO pins, how can I manage them?
Maybe I have misanderstood, but it seems that only XINT1, XINT2 and XINT3 are available.
If more than 1 GPIO is related to XINT1, for exmple, Is there some way to distinguish wich GPIO has generated interrupt?
Or should I use the Capture inputs interrutp? I have not yet studied them.