Part Number: TMS320F28388D
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Tool/software:
Hello,
When I load the dual-core example project in SysConfig, I notice it includes two interconnected SysConfig files (as shown in the attached image). These files are linked in such a way that I can switch between them using the tabs at the top.

In my own project, however, I can only manage to have one SysConfig file for CPU1 and another for CPU2, but I haven't been able to link them as they are in the example project.
Is it possible to configure my project to achieve this kind of linked SysConfig setup? Or would I need to start a new project using the example project as a base to replicate this configuration?
Any insights or guidance would be greatly appreciated.
Regards,